Hi TI,
can i connect IN1 and IN2 directly and use only one GPIO to switch channnel for I2C case?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
can i connect IN1 and IN2 directly and use only one GPIO to switch channnel for I2C case?

Hi Junsong,
Believe this thread is similar to the one here: https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers---internal/f/switches-multiplexers---internal-forum/1097586/ts5a23157-q1-in1-in2-connection
Regardless, IN1 and IN2 can certainly be tied together, this will just allow both switches to change at the same moment. Also, you can also float the NC1/2 pins if you like and will not impact the functionality of your switch as long as this is a low frequency application (otherwise it is advised to tie them to a 50 ohm resistor to GND).
Thanks!
Bryan