This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBT16861: Whether hot plug is supported for SN74CBT16861?

Part Number: SN74CBT16861

Dear 

 Could you please tell me Whether hot plug is supported for SN74CBT16861?

Thanks  a lot.

  • Hey Sam,

    What conditions will the device go under? 
    Is the idea here that the SN74CBT16861 would be powered off then connected to an already existing supply that is powered on? 
    This shouldn't be an issue but would technically exceed the recommended operation supply voltage condition for a tiny bit while it powers up (VCC -> 4-5.5V) so we can't guarantee the performance for that tiny bit of ramp up time. If there are conditions where the device is powered off but you are going to see some input on the I/O's it shouldn't be an issue but note that you will see leakage, as specified in the datasheet:

    Thanks,
    Rami