The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3245A: question for 5ns pulse

Part Number: SN74CBTLV3245A
Other Parts Discussed in Thread: SN74CB3Q3345

Hi Expert, 

There are two solution that customer chosed.

One is SN74CBTLV16212GR, the other one is SN74CBTLV3245APWR.

The question is if they have 5ns pulse need transfer from input to output, is the solution that they chose could accept this pulse?

Or this 5ns pulse would be filter by this two solution.

I saw both devices bandwidth is 200MHz. 

please help to comments here.

Regards,

Mark

  • Hey Mark,

    I wouldn't recommend a 200MHz bandwidth part for a 5ns pulse. This would probably get close to be filtered out. The bandwidth is the -3dB bandwidth so if you start working at the upper edge of the BW you'll find that while there may be some signal output, the degradation may be too large to work with, depending on the use case.
    Typically we recommend a part that has 1.5-3x bw of the frequency you'll be working with.
    So something like the SN74CB3Q3345 could be a good fit here. Bandwidth is 500MHz.

    Thanks,
    Rami