Hi, We are trying to measure the ON-resistance (Ron) of the switch channel.
However the Ron measurement are very different from the spec values (spec values are around 5ohms).
The following are the test conditions:
VCC=3.3V
Measurement path in series connection: 5V <-> terminal-A-of-a-channel <-> terminal-B-of-a-channel <-> 100ohm-resistor <-> GND
OE is connected to GND to turn on the switch channel.
The current flowing thru the above path is measured as 40mA when the channel is turned on.
So the total path resistance is 5V/0.04A = 125ohms. Ron = 125 - 100 = 25ohm.
Just wondering if we are doing something wrong in the above test setup ?
Thanks,
-Jack