Dear team,
Do we have 1 Ch High speed mux solution as below?
Many thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
We do not have a single channel 2:1 mux with the same bandwidth as the TMUX136 but the TMUX136 can still be used with the second channel being tied to ground through a 50 ohm termination resistor to prevent noise. See the FAQ we have on this topic for more information: [FAQ] What to do with unused pins & thermal pads
Thanks,
Tyler
Hi Tyler,
Thanks for your great support!
We DIN the 4 TMUX136 in customer's new project!!
Could you help to review the schematic as below?


Many Thanks,
Jimmy
Hi Jimmy,
Overall the schematic is good but one change would be to ground the COM2 pins with 50 ohm resistors as well.
A more general question is can they utilize channel 2 on each device so that they don't need 8 muxes, only 4? If this was done because each channel needs to be independently switched then the current configuration makes sense.
Thanks,
Tyler