This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3159A: Orderable Part Number and Varying Dimensions

Part Number: TS5A3159A


Hello, 

When a customer order for example TS5A3159ADCKR, how can they know which dimensions they are getting? There are two option with identical part numbers but different lead dimensions. How do we differentiate?

Thanks

Jon 

  • Hi Jon,

    We will get back to you on 7/5 as there is a U.S. holiday on July 4th.

    Thanks!

    Bryan

  • Hey Jon,

    I'm not fully certain how to differentiate which one a customer would receive and i'll look into if there is some way to decide but just to be clear, this dimension isn't the lead dimension this is the tape & reel dimensions (what the devices actually come in when they are delivered) :
    The device themselves will allow follow the dimensions in the datasheet below:



    But it seems there are two different dimensions for the reel that the devices actually come in. Is the customer concerned about the reel dimensions or was this just misunderstood as defining the lead dimensions and as long as the lead dimensions are consistent they are fine? 

    Thanks,
    Rami