Hi,
My customer is facing a problem when using the CD4051 with 3.3V supply, when X3 pin is connected to GND, all the other channels X1-X7 is pulled down to low. The internal short circuit of X3 to other channel may cause this scenario.
Schematic and waveform is as following, 1st channel is output Y when X3 is connected to GND, other 3 channels are channel selection pins. Y has a pull up resistor, which is not drawn in this schematic.
Customer's question is: What reasons may cause to this kind of failure of IC when using 4051, so that they can prevent in future using?


Thanks.