This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiplexer IC Survey Inquire

Other Parts Discussed in Thread: TMUX136, TMUX1136, TMUX1072, TS5A23157

Hi Support team,

We have RF design need switch between 5G and 6G band application.

below as my feature request items:

1. dual output (4CH input to 2CH output)

2. Vcc = 1.8V or 5V

3. control voltage = 1.8V

4. BW need least 100MHz

5. RL = 50 ohm

Could you please help to survey suitable multiplexer parts?

And then please also provide datasheet and price of 500K/month to us refer. Thank you.

Thanks

Regard

Peter

 

  • See here for a search for these parameters.

    The TMUX1072 has overvoltage protection, the TMUX1136 has low leakage current, the TMUX136 is the cheapest.

  • Hi Peter,

    For such an application in 5G/6G, are you sure 100MHz is all you need for such a device? Are they passing anything in the 5GHz or 6GHz range or are you referring to a sub-circuit within this kind of application that does not need these higher speed.

    If you need some higher bandwidth, you can take a look at our TMUX136 for speeds up to 6GHz. For something in the lower frequency range (100MHz), you can take a look at the TS5A23157.

    Let me know if you have any questions on these parts.

    Thanks!

    Bryan