This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3159A: TS5A3159A Used as Switch Application Questions

Part Number: TS5A3159A

Team,

My customer used TS5A3159A as switch, which input signal is AC coupling signa. Needs to check with you if TS5A input can be AC coupling. 

Thank you!

  • Hi Qiang,

    The TS5A3159A can be AC coupled, just note that there are some limitations on how fast of a signal you pass through the device before that begins to be attenuated. The TS5A3159A only supports up to 100MHz maximum (would recommend using a slower signal than 100MHz to give some margin as well), but as long as you do not need anything higher than that, this should work fine.

    Thanks!

    Bryan