Part Number: TMUX6211
Other Parts Discussed in Thread: TMUX1101
Hi Team,
Can you please help to suggest most suitable 1:1 SPST series with the lowest current consumption <1µA with additional requirements below:
1. 3,0V Analog Signal, currents >10mA (3,3V Vcc), 1,8V Logic with Low Ron (<5 Ohm)
2. +5V/-24V Analog Signal, currents up to 100mA, 1,8V Logic with Low Ron (<5 Ohm)
3. +5V/-24V Analog Signal, currents >10mA, 1,8V Logic with Low Ron (<5 Ohm)
For 2 and 3, is TMUX621x good for this?
Thanks for helping
Regards,
Marvin