Other Parts Discussed in Thread: TMUX1308
We are currently considering designing in TMUX4051 in favour of DG4051/HC4051. So far the TMUX4051 is the only 4051 like MUX to be (soon) offered in the very interresting tiny SOT-23-THIN (DYY) package.
The question is now, if we should wait and design in already the tiny package or waste PCB space by designing in TSSOP-16, which is also drop in compatible to CD4051, DG4051 and HC4051 or the like.
Will the SOT-23-THIN and TSSOP-16 versions released to production about the same time, or which delay is to be expected between these two packages ? When is this to be expected ?