This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1208: How much are the input and output impedances?

Part Number: TMUX1208


Hello Sir:

Can you help to provide the input impedance of Sx pins and D pin?

I cannot find it on datasheet.

Looking forward your feedback.

Thanks a lot.

  • Hi Statham,

    Since our analog muxes are passive devices, we do not have an input or output impedance of the Sx pins and Dx pins. For the TMUX1208, we do have an Ron, which is 5Ω(typ), which will be the effective resistance that you will see from S to D on your signal when the switch is on.

    Please let me know if you have any additional questions!

    Regards,

    Nikhil