Hello Team, my customer is missing some specification in the datasheet:
-> specification of the minimum current into error-flags FF and SF for HIGH state (means IOH).
There is a specification in datasheet page 8 with 5mA @ 0.35V (VOL-flag) but customer wants to reduce it to 1mA.
Idea is to use a low current LED with 1mA and 10kOhm pull-up for optical feedback and stable logic level.
MUX will be used in a test equipment hence the LED for signaling.
In the app note there is a 1kOhm pull-up resistor used but this would not fit to the specified 5mA. Any comments on this?
In chapter 8.10 and 8.11 there is a measurement for flag timing but missing value for RPU and CL_xF.
Many Thanks
Josef