This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
I have two question and you may help.
BR,
Elec Cheng
Hi Elec,
The TMUX1309-Q1/SN74HC4852-Q1 are very similar devices, but the TMUX1309-Q1 is essentially a better version of the SN74HC4852-Q1 device in which is has 1.8V logic and more package offferings.
In terms of the competitor part, you can use the TMUX1309QBQBRQ1 (BQB package) as the P2P replacement here.
Thanks!
Bryan
Hi Bryan,
Thanks for your reply! But do you have comparing table between TMUX1309-q1 and SN74HC4852-Q1? That will be very helpful. Thanks.
BR,
Elec Cheng
Hi Elec,
Please see below for comparison.
|
TMUX1309-Q1 |
SN74HC4852-Q1 |
Configuration |
4:1 |
4:1 |
Number of channels (# ) |
2 |
2 |
Supply type |
Single |
Single |
Features |
1.8-V compatible control |
Injection current control |
Break-before-make |
||
Fail-safe logic |
||
Injection current control |
||
Power supply voltage - single (V ) |
1.8, 2.5, 3.3, 5 |
2.5, 3.3, 5 |
Ron (Typ ) (Ohms ) |
59 |
150 |
ON-state leakage current (Max ) (µA ) |
0.8 |
1 |
CON (Typ ) (pF ) |
11 |
6.7 |
Bandwidth (MHz ) |
500 |
- |
Input/output continuous current (Max ) (mA ) |
100 |
25 |
Operating temperature range (C ) |
-40 to 125 |
-40 to 125 |
Let me know if you have further questions.
Thanks!
Bryan