Hi team,
One of our customers uses the TMUX6113 WQFN package, VSS pin connect -11.4V, VDD pin connect +15.5V. But this customer incorrectly connected EP pin to GND and VSS should be connected as per dataset instructions.


The DC/DC power supply -11.4V on some boards was found to be abnormal during the test. However, most abnormal boards will return to normal when -11.4V is reduced to -8.5V or -5V.The board that does not return to normal finds that the -11.4V voltage is short to GND.
The customer wants to know how EP pin are connected to VSS GND pin inside the chip? Can the TI share the information
Best Regards,
Amy Luo