This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi TI,
Question 1: Can TMUX1309-Q1 be used to switch LVDS signals?
Question2:I don't understand why the on resistance is so large, as shown in the figure below:
1. You can use any switch that supports the desired voltages and frequencies. The on resistance of the TMUX1309-Q1 might be too high. Consider the TS3A5017-Q1, or the TS5A23157-Q1/SN3257-Q1 if you need only a 2:1 mux.
2. This device has been optimized for other paramters (that do not really matter for digital signals).
Hello,
The large ON-resistance is just due to the architecture of the device itself. We have other devices that would be more suited for LVDS applications that would have a better RON and bandwidth specification. The ones I would suggest would be the SN3257-Q1 if you need the higher bandwidth or the TS3A5017-Q1 if you do not necessarily need 2GHz of bandwidth and would prefer the 4:1x2 channel configuration.
Thanks!
Bryan