This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6112: Can it be used with Vdd= +7V and Vss = -4.5V?

Part Number: TMUX6112


Hello,

Can TMUX6112 be used with Vdd=+7V and Vss=-4.5V?

Vdd to Vss ranges from 10V to 34V.

Should Vss to GND range from -5V to -17V?

Thank you,

Shimon