Other Parts Discussed in Thread: TS5A23157
Hi,
Customer raised questions below for TMUX136.
- If TMUX136MRSER can be used for 1MHz application? (smbus)
- What is the maximum C_load that TMUX136 can support?
- Is the signal from input to output isolation or transparent?
Customer application:

Smbus speed of master port:(400K to 1M)

Best regards,
Randy