Dear Team,
If we don't use data I/O ports pin of SN74CBTLV3257PWR、SN74CBTLV3245APWR, can we let it keep floating? is there have any risk?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
If we don't use data I/O ports pin of SN74CBTLV3257PWR、SN74CBTLV3245APWR, can we let it keep floating? is there have any risk?
Many Thanks,
Jimmy
Yes; data I/Os of analog switches can be left open (unless you're using very high frequencies); see [FAQ] What to do with Unused Pins & Exposed Thermal Pads?
Hi Jimmy,
For I/O pins, it depends on the application you're using. For low frequency applications, these pins may be left floating without impact on other channels or operation. For higher frequency applications, I advise that the unused I/O's are tied to GND through a termination resistor due to a possibility of noise coupling to the unused I/O's. As Clemens noted, please see [FAQ] What to do with Unused Pins & Exposed Thermal Pads? for more information on this topic.
Thanks!
Alex