There doesn't appear to be a parametric search option for Off-Isolation when searching Analogue Switches which is probably because the off-Isolation vs frequency curve is different for each device.
My application is trying to switch between ultrasonic transducers and requires >75dB Off-Isolation at 5MHz.
Do any of TI's analogue switches support this? I do not mind what switch configuration it has, the circuit I have in mind can be made using 4 SPST switches or two SPDT switches.