Other Parts Discussed in Thread: TS5A23157, , TS5A623157
Hi,
Can the TS5A23159DGSR be used as an IIC switch?
It is assumed that two master devices are used by switching for a Slave Device.
In that case, the power supply of TS5A23159DGSR is 3.3V.
IIC communication assumes 1.8V 400kHz.
I think that it can be realized with the circuit diagram below,
is there any problem in using the TS5A23159DGSR?

Thans,
HOTA