Other Parts Discussed in Thread: SN74LVC1G07, SN74CBTLV1G125
Hi
It is recommended that the following output is open drain IC SC70-5 SMD 3.3V
Or a single bit switch with OE# pin SC70-5 IC?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hi Alex
The customer is looking for a single switch with the following p2p but not buffer, because both sides may pull low at the same time, when the right side wants to pull low, if the left side is high, it cannot be pulled down You can also recommend without p2p, thank you

Hey Gareth,
Is a SPST (1:1 switch) like the SN74CBTLV1G125 what you're looking for here? What are frequencies and use case here?
There is also an automotive version of this device I listed above.
Thanks,
Rami