This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A44159: EVM?

Expert 6630 points
Part Number: TS3A44159
Other Parts Discussed in Thread: 16DYYPWEVM

Is there an EVM for this part? Or a similar part with EVM?

thx

Andreas

  • Hi Andreas,

    May I ask which package you're using? There is no EVM for this part, but you can use this EVMThe 16DYYPWEVM  is a test board for SOT-23 THIN (DYY) and TSSOP (PW) packages. We also have a leaded adapter which allows for quick testing and breadboarding of TI's 5, 8, 10, 16 and 24 pin leaded packages. 

    Let me know if this helps!

    Thanks!

    Alex