Other Parts Discussed in Thread: ISO7740
Hi Team,
if S pin and D pin is isolated with the power pin and SEL pin, whether this device can work? In this situation, power pin and SEL pin sharing the same GND.

BRs,
Francis
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Francis,
From my understanding this might be the information you are looking for.
This device will not pass a signal on a unselected channel ex(S1 to D1) What controls the path be connected or disconnected is the control logic pins(sel1-sel4) and the power pin isnt involved in channel selection. Also ther is a ground pin on this device which ever grounds the whole device.
Thanks and Regards,
Kameron
Hi Clemens, Kameron,
Sorry for the confusion, customer uses TMUX8212 in a isolated situation means the S/D/VDD/VSS/GND pins have a common power ground, but the logic control signal SEL pin belongs to a digital ground(isolated from power ground). Currently, they add a ISO7740 for meeting this requirement, due to we think SEL pin must have a common ground with VDD/VSS. Could you please help me check whether it is right? And if customer don't want the ISO7740, what can they do to meet the necessary requirement - power side electrical isolation? Thanks a lot.
BRs,
Francis
The SEL voltage must be referenced to GND; see the VSEL specification in section 7.3.
In this application, you indeed need an isolator for the SEL signals.