Hi
I want to use sn74cbtlv3251 mux in my new design.
B1 to B8 pins are input,and A is output.
When OE(pin 7) is high, what is the state of output ?
Is it floating, high impedance or pull low ?
Thanks
BR,
Hank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I want to use sn74cbtlv3251 mux in my new design.
B1 to B8 pins are input,and A is output.
When OE(pin 7) is high, what is the state of output ?
Is it floating, high impedance or pull low ?
Thanks
BR,
Hank
Hi Hank,
Clemens is spot on here - when OE is pulled high, the output is in a disconnected state which in this case means it will remain floating unless you manually set it as a certain level via a pull-up or pull-down resistor.

Let me know if you have any other questions!
Thanks!
Alex