Part Number: TS3L501E
Other Parts Discussed in Thread: TS5A22362
Hi,
One of our design circuit uses TS3L501E to switch b/w two Ethernet networks. I have the following questions:
- The post here says: "Yes, driving the ethernet lines while the device is not fully powered will damage the part." Does it mean if no power is applied to IC and if one connect the RJ-45 connector (other end connect to say a router), will the IC get damaged? Similarly is the case if we power down the device via PD pin pulled low.
- Our circuit uses 5V MCU. does the following resistor divider circuit can be used to drive SEL and PD pins (to convert from 5v to 3.3v)? The power source of IC is kept at 3.3V.