Hi Sir,
customer want to know differenr voltage drop V.S current in different Vgs for level shift( the curve in the figrue below), and there no similar curve in SPEC.
is there any information on this can be provide?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
customer want to know differenr voltage drop V.S current in different Vgs for level shift( the curve in the figrue below), and there no similar curve in SPEC.
is there any information on this can be provide?

Hello Tommy,
This device is a bidirectional device which means signals can pass from source to drain but can also be sent drain to source. Also this switch can be modeled as a resistor.
Are you looking for a level shifting device? If so I can definitely you help from that business unit.
Regards,
Kameron
The TMUX136 is a signal switch, i.e., it is not meant to pass large currents. It is characterized by its on-resistance (see section 6.5 and figure 6-1).

The voltage drop for the specified worst-case test conditions would be 13 Ω × 8 mA = 0.104 V, but in practice, your circuit is likely to use a lower current, and the actual resistance would be lower.
Hi Tommy,
I agree with Clemens on this. The Tmux136 is characterized by Ron vs voltage input so there is no curve like the one you provided. However the mux can be modeled as a resistor and the solution Clemens described is applicable.
Thanks and Regards,
Kameron