Dear Ti
Custom board, the switch connect as MAC to MAC with SGMII. A core is linux with VMac. The speed is 1000M as default.
so it is 1000M in A core eth0.
Question:
How to set the speed of eth0 as 100M?
TDA4 with SDK8.4
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Ti
Custom board, the switch connect as MAC to MAC with SGMII. A core is linux with VMac. The speed is 1000M as default.
so it is 1000M in A core eth0.
Question:
How to set the speed of eth0 as 100M?
TDA4 with SDK8.4
thanks!
customer want to send 100Mbps traffic from A72 to CPSW-9G with max speed 100Mbps
but A72 Linux can not set speed to 100M,
so how to set the port connected to Reltek Switch to 100Mbps