This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6219: VDD=5V VSS=-24V application scenario

Part Number: TMUX6219


Could I use TMUX6219 in scenario such as VDD=5V and VSS=-24V? I don't find clear answer in datasheet.

In this case, does there any other considerations to notice?

If TMUX6219 could not fit the design, could other device make it or not? Need you help here, thanks a lot.