This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX7202: Switch status when no power is present

Part Number: TMUX7202


Hi all.

I am planning to use TMUX7202 as a switch to short the output of a circuit to the ground during start-up.

I am wondering, if I set SEL pin to low when no power is present, is switch in closed or high impedance state?

Thank you.

Derun

  • There are clamping diodes to the power supply rails. When powered off, you must not apply any voltage to the I/O pins. (See the absolute maximum ratings.)

    TI does not make any switches that are guaranteed to be closed when powered off.

  • Hi Clemens,

    Thank you for answer. I think it is mentioned in the datasheet that applying voltage to only SEL pin is ok without any power. Fail-Safe Logic circuitry allows voltages on the control pins to be applied before the supply pin, protecting the device from potential damage. Anyway, you answered my question, thank you.