This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A27518E: data rate inquiry

Part Number: TS3A27518E


Hi, TI support team

TS3A27518ERTWR band witdh is 240Mhz.

How much data rate is supported based on QSPI 6bit?

Thanks.

Regards,

MJ

  • This 240 MHz value is the analog −3 dB bandwidth (see figure 6-11).

    Digital signals are not sine waves but square waves and require more harmonics, so I'd estimate the limit to be somewhere below 100 MHz. Please note that any resistance or capacitance (e.g., long traces) will reduce the speed further.