Part Number: TMUX4052-Q1
Does this switch support ISO7637 5b test
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes, the current-limiting resistor will prevent the TMUX4052-Q1 itself from being damaged. Your circuit still needs to be able to handle the current flowing into VCC. (If the VCC voltage floats up, all devices connected to it might get damaged.)
Another question:Is there component add on Vd/Vs can improve the Voltage range? Datasheet shows Vd/Vs can withstand max +0.5V than VDD. If we conduct short to bat test VDD might be 13.5V and we will use anther source add to Vd/Vs about 16V, so is this possible?
There are diodes between the I/O pins and the supply rails. If you apply any voltage more than 0.5 V beyond the rails, a current will flow, and the diodes will clamp the voltage to their own forward voltage.
You could add external diodes in parallel with the internal ones. (Use a resistor between the external diode and the pin so that most of the current flows through the external one.) You can size these external diodes for whatever current is needed.
When there is a high voltage at z02.CC1/2, then a current flows through R9733, and the voltage drop over R9733 will make the voltage at the chip's pin higher than the supply voltage (z02.U140P_USB3).
Drop that resistor, and add series resistors between the pins (DB and S0A) and the diodes.
(And VDD needs a low-impedance connection to the supply; remove R9730.)
Sorry; my recommendations were for overvoltages at the I/O pins, but you want protection against overvoltages at the supply.
The only way to protect against overvoltage at the supply are TVS diodes that clamp to a low-enough voltage.
Vdd high voltage problem we will use another stable power. For I/O pin I mean you suggest series resister on CC1/CC2 pin for limit current, but we can't do that, we add schottky diode to prevent CC1/CC2 voltage from exceeding Vdd and prevent current from passing through