Part Number: TMUX6208
Hi,
I have connected the signle ended analog input signals (0-5V) to the Source pins of TMUX6208. So, I have provided 5V to VDD pin of the IC and VSS is directly tied to GND. Is it fine?
Or Shall I need to connect VSS pin to -5V rail? If -5V is not required for VSS pin, then is it fine that I have tied VSS directly to GND or I need to connect VSS pin to GND through a capacitor mentioned in datasheet?
Please suggest.