This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3A27518E: Can this part to be used for Dual host?

Part Number: TS3A27518E


Hello,

I have the query about the application of TS3A27518E. In the datasheet it shows that this IC can be used to multiplex the SDIO port for two SD-Cards and one Host controller. But in our application we have two Hosts and one SD-card. So, can I use this part for dual host controller and one peripheral? 

Just for the information - I used TXS02612RTWR earlier but it doesn't work as TXS02612RTWR has single directional clock and not able to fulfill our purpose of two host.