When using TMUX1574 to connect SPI from Microcontroller to two devices are pull-up resistors required on the SPI signals on each device?
If there are no pull up resistors then the SPI signals to the un-selected device will be floating.
This diagram is from the datasheet:

Also is it possible to use two TMUX1574 to connect four SPI devices to a microcontroller as shown below?
SEL and EN signals will be controlled by port bits on microcontroller.