Other Parts Discussed in Thread: TMUX136, TMUX1072, TMUX2889, ISOW1432
Hi TI,
We require your support in identifying a Mux/Switch/SSR For switching between RS422 signals.
Description:
We are in the process of developing a customized board for military and aerospace applications. The board involves two pairs of RS422 signals: a primary pair and a redundant secondary pair, both operating at a rate of 2.5 Mbps(2.5MHz) the secondary pair acts as a backup and is activated only if the primary pair malfunctions. The driver end utilizes AM26LV31ESDREP. For isolation purposes at the receiver end, we employ an optocoupler to convert the RS422 signals to LVCMOS signals, which will then be connected to an FPGA. To switch between primary and secondary pairs, we've opted for the TMUX4827YBHR IC. The optocoupler requires a minimum of 1.8V across Anode and Cathode to detect a high voltage. An image of depicting the electrical connection of the circuit is attached with this query.
Issue:
The output voltage of the TMUX4827YBHR matches the input voltage across the frequency range of 10KHz to 120KHz. The input, coming from AM26LV31ESDREP, is approximately 4Vpp (differential).
The TMUX4827YBHR output stays equal to the input up to about 120KHz. Beyond this frequency, the output voltage starts to deviate from the input and begins to decline. Around 290KHz, the TMUX4827YBHR output reaches approximately 1.75V(Differential), which is just enough for the optocoupler at the receiver end to detect the signals, despite the input still being 4Vpp (differential).
However, beyond 290KHz, the output drops significantly below 1.75V. Consequently, the optocoupler at the receiver end struggles to recognize the transactions occurring above 290KHz.
Also, we are using a current limiting resistor at the anode pin of opto-coupler. Since the O/P voltage of TMUX4827YBHR is changing from 4Vpp differential (@10KHz) to about 1.2VPP differential (@2.5Mhz), the forward current If is also varying significantly.
Query:
Can you please suggest a suitable part, such as a switch, multiplexer (mux), or solid-state relay (SSR), that would better fit this application and address the issue we are facing with the TMUX4827YBHR?

Regards,
Sameep