Part Number: TMUX1208
I have 2 questions as below.
(1) If induced voltage is generated at TMUX1208 as shown in below, the IC will exceed its rated voltage, there is a possibility of failure.
→ Can you predict what operating mode will be in case of failure? Please provide as much detail as possible.
(2) If a failure occurs such as case (1), is it possible to recover by turning the power back on?
Best regards, thank you.
----------------------------------
(1)TMUX1208にP3 , Fig.2の様に誘導電圧が発生することで、ICが定格電圧を超えるため、故障する可能性があると思います。
→故障する場合の動作Modeがどうなるか想定できますか?できるだけ詳細に教えてください。
(2) ,(1)で故障する場合、例えば電源再投入して復帰動作するということがあり得ますか?