Other Parts Discussed in Thread: TCA5405, TCA9536, LMH6720, TCA9537
Hello
I wanted to replace the DG884 8 x 4 Wideband Video Crosspoint Array muxtiplexer with the LMH6580.
I am missing a function on this product, the 4 DISABLED outputs function.
Address A3 functions as an output turn-off command. There
are four open-drain DISABLE pins that are active low when the
particular output is off. They are designed to interface directly
with the disable pin of the CLC410 current feedback op amp.
Do you have an 8x4 Analog Crosspoint with this function?
Thank you for your help.
Please find attached the DG884 datsheet see page 3 bit A3