Other Parts Discussed in Thread: LMH6572
I am feeding STANAG-format single ended signal to cross point switch
Top LEVEL Block Diagram:
When cross point switch is in power down state, Sync and Active Video of signal is degraded at the input of the crosspoint switch.(Reason - Since few input signals shall bypass the switch at initial state and fed to MUX)
But, when the crosspoint switch is active, signal founds okay at input of the crosspoint switch.
Schematic and Oscilloscope pics are attached below for reference
SCH:
Observations:

H-SYNC should be around 300mV ideally as per STANAG format, But if the crosspoint switch is in power down mode, level got reduced to 180mV. Additionally, the rise time of active video also degraded
Kindly, update regarding this query as early as possible
Thank you.