This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1511: protection when short to 16V

Part Number: TMUX1511
Other Parts Discussed in Thread: TMUX6111

Based on below application, if the output short to 16V, can the tmux1511 be protected without the diode.

Assume there is body diode inside the input of tmux1511, and current is limited by resistor b to make it smaller than 25mA.

I am not sure if it's the right architecture inside tmux1511, please confirm.