Other Parts Discussed in Thread: TMUX7221, TMUX4827
Hello,
I have an application where we have one RFID Transceiver (STMicro ST25R3916B) which outputs a differential antenna signal that then goes through an antenna mux to select one of 16 different PCB trace antennas. Antennas are small, about 1" in diameter and read distance is very close, maybe 0.5". Currently the antenna mux is just 16 different DPDT relays controlled by an MSP430. But we'd like to replace the relays with a silicon based solution for noise and cost. Would the TMUX6221 work? The antenna signal is bi-directional, about +-6V; see attached. I figure that we would need to power the chip with +/- 15V so there's plenty of headroom. The Ron of 2 ohms isn't a problem since I'm already attenuating both signals by a few ohms. According to the datasheet the -3dB bandwidth is 45MHz so it should be sufficient. If it matters, duty cycle is low, <1%. Finally, control logic voltage is 3.3V nominal but I can adjust that to whatever is needed.
I see also that there's the TMUX7221; is that just the same thing but can handle higher voltages? Any benefit?
There's also the TMUX4827 but that's in a tight 0.4mm pitch BGA which would require a higher spec board. It has a bandwidth of 72MHz but then Figure 6-22 in the datasheet says that above 50kHz the voltage swing is limited to +/-2V so that part is kinda sus.
Finally, how can I get samples of this or a development board to test? This would be a change to a product on the market already and volumes are decent.
Thanks,
Derek