This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX9616: 220V switches without bleed resistor

Part Number: TMUX9616

The 220V analog muxes have really powerful use cases in test and measurement. However, I noticed the two TMUX9XXX products that are in preview have bleed resistors on the signal path. Are these always on? I have an application where I need to pass high voltage, but the signal can't be loaded down. Will all future versions have the bleed resistors? It would be excellent if there were some switches internally to turn them off for applications where it isn't needed.