This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use in this scene: I use 1.8V for V+, but 3.3V for IN1 and IN2. Can TS5A23157-Q1 work well?
No, the absolute maximum ratings forbid this.
The SN3257-Q1 supports input voltages beyond the supply.
Hello,
I agree with Clemens answer and to understand what to do with the unused pins in your application please look at this FAQ.
Regards,
Kameron
Hello Yao
Clemens is correct and please ask any additional questions if you have them.
Regards,
Kameron
you say figure 6-1. I can not find figure 6-1 in the datasheet. Can you paste the figure 6-1 on this question post?