Other Parts Discussed in Thread: TS5A23166, TS5A21366
Hello,
Does this device have positive clamping diodes on VIN?
Basically, trying to understand if I can apply 5V to VIN or NO when VCC is 3.3V. I read the footnote that "The input and output voltage ratings may be exceeded if the input and output clamp-current ratings are observed" but it's still pretty unclear.
Thanks,
Michael