Other Parts Discussed in Thread: TMUX1511
Hello,
I am using the 4066 as below to switch RX/TX to different ports:

At initial time while all the control lines are 0, 5V to ERXD, (5V from the TX of the connected serial port, from another system) causes mis-operation.
Mis-operation is that this is a custom board on a raspberryPI hat, so basically RXD is connected to RPI4s RXD port. When the rpi boots, all the control lines are zero.
I have purposefully placed rx/tx combinations thinking it was single direction switch, so directionality is preserved.
Taking the below diagram into account, how can 5V at input A, while C being low, cause mis-operation.