This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DPDT device

Other Parts Discussed in Thread: TPS22810, TPS2124

Hi team, 

just want to check if there is >=7.5V DPDT ( double-pole double-throw) , >=1A device. Thanks. 

BRs

Given 

  • Hello Given,

    So your are asking for a 1:1 2channel switch like this

    1.Does it need to  support a 7.5V supply voltage(VDD) or 7.5V signal (source to drain)?

    2. Does this device need to support 1Amp current through the signal path or survive 1amp current fault situtaion?

    Regards,

    kameron

  • As far as I understand, a DPDT switch has two 1:2 channels:

    Normal switches are designed to handle analog and digital signals, and small loads; they cannot handle 1 A.

    What is your application? There is no integrated device that has four 1 A I/Os. If you want to switch between two power sources, you might be able to use two power muxes like the TPS2124. The most general solution would be to use four load switches like the TPS22810.

  • Hi Kameron, 

    The device is like Clemens says below. Thanks. 

    BRs

    Given

  • Hi Clemens, 

    Thanks for your reply. That's what my customer want. application is in smart watch. 

    customer think two channel integrated will have better consistency than two different device.. Thanks. 

    BRs

    Given