Hi Team,
What is the max load current consumption of TS3A27518EPWR.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Then what is the max Current consumption when Vcc is 3.3V. Or how to calculate power dissipation of TS3A27518E
For calculating the power dissipation, see [FAQ] How to calculate max junction temperature (Tj max) and max power dissipation for an analog switch.
Hi Chaitanya,
Thanks for reaching out here. In addition to Clemens comment on calculating power dissipation, I'd like to start with linking an app note we have on Preventing Excess Current Consumption on Analog Switches.
Probably the most important takeaway here is that in a typical application, you'd have high current consumption when the control input is between GND and VDD, and very low leakage when control input is at GND or VDD. The good news is that you've already picked a device with 1.8V logic, so you won't run into this issue - just something to note for the future.
If you need any other help or insight here just let me know!
Regards,
Alex