Other Parts Discussed in Thread: TMUX1574
Hello,
I have downloaded IBIS model for TMUX1511 for Signal Integrity simulation.
However S1,S2, S3, S4 and D1, D2, D3, D4 pins are defined as inputs only.
As per datasheet and our application, I can use these pins as output also.
However IBIS model do not define these pins in output configuration.
Can you check and update the IBIS model for S and D pins in output configuration also, so that I can start the simulation.
Regards,
Surendra