Other Parts Discussed in Thread: TMUX1511,
Hi ,
This part doesn't support 1.8V VCC, Is there an alternate?
I am looking for a part which support 1.8V for VCC & Data IO.
Thanks
Kanava
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
This part doesn't support 1.8V VCC, Is there an alternate?
I am looking for a part which support 1.8V for VCC & Data IO.
Thanks
Kanava
Hello Kanava,
Here is our parts portfolio filtered for 1.8VCC and I/O:
https://www.ti.com/switches-multiplexers/analog/products.html#3306=1.8&
Are there any other specific parameters you are looking for? If so I can narrow it down to a few parts instead of a long list.
Thanks,
Nir
Thanks, I am looking for (SPST), 20-channel FET bus switch which support 1.8V for VCC and Data IOs.
Hello Kanava,
Unfortunately, we don't have a 20-channel device with such parameters and configuration.
The highest channel we have with those specs is 4, which is the TMUX1511: https://www.ti.com/lit/ds/symlink/tmux1511.pdf
You can combine a few 1511's together and turn them into a 20 channel device.
Thanks,
Nir
Hi Nir,
Ok, Thanks. I will check that.
one more question, Can I use 'SN74CB3T16210-Q1' part for the below config
VCC - 3.3V
Data IOs -1.8V
Hello Kanava,
Yes, you can please see below operating conditions:
Thanks,
Nir