Hi,
I am looking for some clarification on the maximum allowable current into the TMUX136.
The datasheet states it is +/- 20mA Continuous. What is the maximum pulsed current and duration of this ? or is it simply that the pulse current x dutycyle should not increase above specification?
Let's say I have a LVTTL signal with +3v3 and a 100R resistor on the output of the MUX, if the duty cycle is 50% then average current would be below 20mA. Is this what the datasheet means by maximum allowable continuous current?